This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

AMC131M03: Residual current monitor (UL2231-2)

Part Number: AMC131M03


Hi

There is residual current standard(UL2231-2) in the EV AC charging station(Level 2)  specification.

I want to use AMC131M03 to monitor residual current.

Is it possible?

I have an AMC131M03EVM and can I monitor  residual current on AC with this?

If possible, please let me know how.

Thanks

  • Hi David Kim2,

    Due to the holiday week here in the US, please expect a response during the week of January 2. Thanks for your patience

    -Bryan

  • Hi David,

    Thanks for your patience. AMC131M03 ADC can be used to measure any voltage or current signal including residual current measurement (detection and monitoring) in EV charging stations as long as the signal is within the range and the ADC operates in the recommended conditions in the following table:

    Also, the power supply and inputs should not violate the specifications in the following table so that the safety of ADC can be guaranteed.

    AMC131M03 datasheet shows typical application and block diagram for current and voltage measurement with AMC131M03 ADC, please see section 9.2, figure 9-4 and 9-5 in the datasheet here.

    The app notes and reference designs in the this link could be a good reference for you:    EV charging infrastructure

    Regards,

    Dale