Part Number: TSW14J57EVM
Other Parts Discussed in Thread: ADC12DJ3200EVM
Hi, Teams,
We have an experiment enviroment with ADC12DJ3200EVM, TSW14J57 and HSDC Pro 6.0. We tested the trigger option of 2 cases: 1) external trigger 2) software trigger. Both of them didn't work at all.
Our steps are as follows:
1. Power the boards and set the GUI of ADCEVM.
2. Download the firmware of ADC12DJXX00_JMODE[n]_trigger.ini. (we tested jmode0 and jmode2)
3. Set the trigger option of 2 cases. In the case of external trigger, a 0.1Hz pulse (High Voltage 1.8V, Low Voltage 0V, pulse width 20ns) is connected to the trigger_in, but it was said "Waiting for user input". In the case of software trigger, it was alarmed "No trigger occurs".
We are so confused. If there something else we need to do with the board?