Other Parts Discussed in Thread: DAC5682Z
Hi,
I am a new user for the chip DAC5682Z. In our project, the chip DAC5682 is used to output our calculation results, where every data is 64-bit. In a reference design, a 64-bit data is divided into four 16-bit data through DDR mode, and then the 16-bit data are input DAC5682(Pin N0--N15).The input data are generate by FPGA at 100MHz, and DAC clock is 200MHZ. My questions are:
(1)what are the final conversion results? 16-bit input data or 64-bit data?
(2) I watch the outputs through an external oscilloscope (100MHz, 1GS/s), when the input data is a sine wave, the output is stable. If the input others, the output is distorbed. what is the problem?
(3) DAC5682 has two channels. From the function diagram, there is only one input (Pin N0--N15). Are the outputs of two channels same ?
Thanks,
Steven Tan