This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

AFE5832: Please provide AFE5832 and AFE5832LP and the specific differences.

Part Number: AFE5832

Please provide AFE5832 and AFE5832LP and the specific differences. There are two types of devices and equipment, and only AFE5832LP complete information.

  • Hi, 

    AFE5832 and AFE5832LP have different architectures, different register maps but have the same pinout and support 32 channel input.

    AFE5832 

    AFE5832LP

    Key difference is in power and noise. AFE5832 is higher power but lower noise. AFE5832LP is lower power but higher noise. The specific details are available in the one page datasheet of both devices which is available online. I am attaching a snapshot here. You can request the full datasheets here and here

    Thanks, 

    Karthik