This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

ADS8686SEVM-PDK: ADS8686SEVM-PDK:

Part Number: ADS8686SEVM-PDK


Hello
Selected to order ADS8686SEVM      Does it includes the 16 channels ADS8686 board and the ADS8686-PDK PHI board or do I need to order them as two separate items.

As paired they are a single item in MOUSER. 595-ADS8686SEVM-PDK
What is the PN if we order direct from TI


  • Hi Avner,

    Welcome to TI E2E forum. We only have one part number to order:  ADS8686SEVM-PDK which has included ADS8686SEVM board and the PHI controller board. TI or TI's authorized distributor does not individually sell the PHI controller board.

    Regards,

    Dale

  • Dear Dale Li
    Thank you for clarifying this issue.
    Please advise , Can we stream continuously data of all 16 channels through the USB to a host PC, or is there a limit of buffer size 
    If there is a limit - please define the size or ways to overcome such limit. I need 3-5 seconds records, of 16 channels 5-15KHz BW.
    May we get mechanical size drawings of the ADS8686SEVM-PDK boards.
    Best regards
    Avner 

  • Hi Avner,

    The setup (EVM GUI and PHI card) does not support not a real-time data collection. I'm checking with team to get the details about the limitation and I will get back to you as soon as I can.

    Regards,

    Dale

  • Hi Avner,

    If you are considering to use the EVM GUI software and PHI controller card to collect data from the ADS8686SEVM, this data size is limited to 1048576 samples. The EVM-PDK with PHI card are not intended to be a final product, or test platform, outside of its intended application purpose to work with our EVMs for ADC evaluation purpose.  

    Regards,

    Dale