Other Parts Discussed in Thread: AFE5832, AFE5832LP
Engineer of AFE5832:
I recently encountered two problems when debugging the AFE5832 chip.
Question 1: The TX_TRIG signal seems to be invalid, because I used the AFE chip to receive 32 signals, the first 16 channel signal and the last 16 channel signal can not be synchronized, they have a fixed misalignment. What should I do to ensure that the TX_TRIG signal is valid?
Question 2: In the following figure, I use the ramp test mode of AFE5832, but there are some problems with the received channel data, but some channels are completely correct, I can't find the reason.