With a reference voltage of 2.4V and a gain of 6 V/V, I should have a signal range between -400 mV to +400 mV, but the ECG signal has a range between -1 mV and +1mV because of default do I have such a large range? in this way the signal will always be very small