Part Number: ADS9218
Other Parts Discussed in Thread: ADS9219, ADS9224R

Hi team, you can see the above picture I used such a circuit to simulation the ac and noise performance of the ads9218,with the fin=2KHZ ,amp=3.6V sine wave .and the SNR test result equals to 133dB, but from the datasheet , the SNR in such test condition should be 95.1dB, why there will be such obvious deviation between this?