This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

DAC81416EVM: 无法配置16通道输出电压

Part Number: DAC81416EVM

你好,我想用FPGA控制DAC81414EVM评估板16个通道输出不同的电压值,发现无法配置成功。
硬件连接如下:
J12的1脚和2脚连接
J10的2脚和3脚连接
J9的1脚和2脚连接
J11不端接(为了测试使用内部电源)

J7的3脚接GND,4脚接+3.3V,5脚接+5V,6脚接GND,7脚接+12V
J8的1、2、3、4、7、8、9、10分别用杜邦线和FPGA的IO管脚连接

FPGA寄存器配置顺序如下,SPI的时钟只有几兆.
0x03 0x0A84
0x04 0x2000
0x0A 0x9999
0x0B 0x9999
0x0C 0x9999
0x0D 0x9999
0x09 0x0000
0x02 0x0001

0x10 0x9000
0x11 0xA000
0x12 0xB000
0x13 0x4000
0x14 0x5000
0x15 0x6000
0x16 0x7000
0x17 0x1000
0x18 0x2000
0x19 0x3000
0x1A 0x4000
0x1B 0x5000
0x1C 0x6000
0x1D 0x7000
0x1E 0x7000
0x1F 0x7000

测试发现TP12引脚能够输出2.5V。但16个通道并不能输出电压。
请问
1、上述接线和寄存器配置内容和顺序是否存在问题。
2、如果没有没有问题为啥配置不成功。