Part Number: ADS1282
Hello,
I am currently using the ADS1282 in my design in pulse mode. The design is composed of two external multiplexers, which provide the input voltage to the ADC for both channel 1 and channel 2. During my acquisition cycle, I perform a continuous switch of the external mux in order to set the data to be sampled.
1) If I use the SINC filter only, how long do I need to wait from the ADC internal mux selection and the first valid sample? Does this delay need to be applied also in case of external mux switch when interal mux keeps fixed?
2) How the delays change in case of using SINC+FIR mode?
Thank you