Other Parts Discussed in Thread: REF5025, REF5040, LM4140
I'm looking to substitute the obsolete Analog Device max1298 ADC with the TI ADS8028.
In max1298, the 5V analog input span is obtained from a 2,5V voltage reference.
with the ADS8028 ADC I want use a 4,096 voltage reference and it is not possible to enable the ADS8028 external voltage reference after disabling the internal voltage reference of the ADS8028.
1) in EVM datasheet
https://www.ti.com/lit/ug/sbau198a/sbau198a.pdf?ts=1706520965337
at pg.10 it is written:
"The user should avoid connecting any external voltage reference to the ADS8028 before a serial write to the ADS8028 control register disables the internal reference source. Providing an external source prior to this communication draws additional current from the external source. The ADS8028 internal protection circuitry limits this current to 20 mA".
At the same time, in the EVM electrical scheme the external Vref can be directy connected to the ADC Vref input.
also in the ADS8028 data sheet this warning is reported and the ref5025 is suggested, but in this case the VREF is 2,5V (the same of the internal reference.
I wish to use the external reference ADR444B (Analog Device) about 4V voltage reference (High output source and sink current +10 mA and −5 mA, respectively).
I need help to find the right interconnection scheme to use the 4,096 V voltage reference in input to the ADS8028 Vref pin.
thank you in advance for your help.