Part Number: ADC12DJ5200RF
Hi,
Can 1.9V be used for SPI and 4 pins for frequency setting when it is connected 1.8V I/O in FPGA?
Thanks.
This thread has been locked.
If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.
Part Number: ADC12DJ5200RF
Hi,
Can 1.9V be used for SPI and 4 pins for frequency setting when it is connected 1.8V I/O in FPGA?
Thanks.
Hi David,
I'm not sure what you are asking. The ADC can accept up to the lower of (VA19+0.5V or 2.35V) for the SPI lines or NCOxx pins. If you are asking about if whether the IO of the FPGA can accept the 1.9V CMOS logic of the SDO line, then that is dependent on the FPGA. I do not know.
Thanks, Chase