Part Number: TX7516EVM
Hi,
I just started working on the TX7516EVM and were following the user guide.
I set the power supplies as specified on the user guide and the +5V supply showed 2Vdc & 200mA.
I’ve sprayed some freeze spray on the eval board just to see where this short circuit is coming from and 3 ICs immediately unfreezed -> U2, U3 & U13
Then I tried to power up the 2V5 & 3V3 independently using an external power supply. I have 50mA on 2V5 and >450mA on 3V3.
I suspect U13 to be the source of our problem but I might be wrong.
Thank you