Part Number: ADS114S08
Other Parts Discussed in Thread: ADS1158, ADS1258
Hello all.
We are developing an accelerometer reader with 12 channels.
For the data convertion, we are using ADS114S08IPBSR ADC converter.
The aquisition frequency that we need, on each channel, is 600 hz.
After some analisys, I checked that the max sample rate of ADS114S08IPBSR is 4000 SPS.
So, if I need to multiplex the channels (reading one channel per time), the max frequency that I can have is 4000/(nbr of channels)?
Is it possible to read all the channels at the same time without multiplexing them?
Thanks in advance.