Dear engineers,
We use AFE5832LP for the design.
We want to divide the ground into two different grounds: AVSS (analog ground) and DVSS (digital ground) for better performance.
But we are confused about which type of ground the pins belong to.
In the pdf file, we can find the pin and its "Rail reference". The questions are:
1. If the "Rail reference" is only about “AVDD”, it means that these pins will be associated with the AVSS (analog ground) and wired on the AVSS (analog ground)? The pins use the AVSS (analog ground) as the reference point?
Such as the "INPx", "INMx", "TGC_SLOPE", "ADC_CLKP", "TGC_UP_DN" and so on.
2. If the "Rail reference" is about “AVDD”and "DVDD", which ground are these pins wired on? and which ground to use as the reference point?
Such as the "SDOUT", "SCLK", "SDIN", "RESET", "PDN_GBL" and so on.
3. If the "Rail reference" is only about “DVDD”, it means that these pins will be associated with the DVSS (digital ground) and wired on the DVSS (digital ground)? The pins use the DVSS (digital ground) as the reference point?
Such as the "SEN", "TX_TRIG ", "DOUTPx" and so on.
Thanks for your help.