This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

ADC12D800RF: Using both AutoSync and TimeStamp

Part Number: ADC12D800RF

Hi team,

In the ADC12D800 datasheet Table6-30 and 6-15,
When Addr: Eh Bit 2:Enable Slave is set to Slave Mode,
is it OK to use TimeStamp by setting Addr: Eh Bit 0:Disable Reset to "enable DCLK_RST functionality" and
Addr: 0h Bit 3:Time Stamp Enable to "enabled"?

My customer would like to use both AutoSync and TimeStamp.
Please let me know if TimeStamp is available when setting Slave mode to use AutoSync.

Best regards,
Kazuki Itoh