This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

DAC80502: issue in SPI clock pin of DAC80502EVM

Part Number: DAC80502


I am using DAC80502EVM module and interfaced it with LAUNCHXL F28379D using SPIA. Whenever I try to send 24bit data to change the DAC module output it does not change automatically. Instead I have observed that if I connect an unloaded (not connected to DSO) voltage probe between TP1 (CLK input of the module) & TP2 (ground), then only I can change the output of DAC by sending 24bit data using SPI. I realized this is may be due to some noise in the clock channel. I have used a 10nF capacitor to filter out noise, but it is of no use. The module can only work if a unloaded voltage probe is connected as mentioned above. Kindly help in this regard. 

Thanks.