Hello,
I am working on a prototype that uses the following component, ADS1292R for ECG acquisition.
I want to upgrade my prototype by introducing a two-channel ECG using ADS1292R.
I have gone through the following user guide, ADS1292 User's Guide. On the page 51 of this user guide, I saw a reference schematic. On a side note on the same page the following is written,
" Note: For two channel ECG Do the following modification
(1) Mount 51K resistor in place of R71 and R63
(2) Mount 0 Ohm resistors in place of C48, C46, C49 and C50
(3) Make following components DNI R66, R64, R72, R62, C47,C45,R70 and R69 "
So I have made a rough schematic diagram on how this would look like,

Can anyone confirm that this is correct?
If yes then I will design the schematic and on this same thread update for the schematic review.
Thanks and Regards,
Mohin Shaikh