Other Parts Discussed in Thread: ADS42LB49, ADS42LB69
Dear Sir/Madam,
As per datasheet 8.3.5: Output Data Format
FFor a positive overdrive, the output code is 3FFFh for the ADS42LB49 and ADS42LB69 in offset binary output format; the output code is 1FFFh for the ADS42LB49 and ADS42LB69 in twos complement output format. For a negative input overdrive, the output code is 0000h in offset binary output format and 2000h for the ADS42LB49 and ADS42LB69 in twos complement output format.
Both ADS42LB69 and ADS42LB49 have the same overdrive code; if so, where do the 14 and 16 bit digital data come in?
As per section 9.2.2.1 Analog Input
Each input pin (INP, INM) must swing symmetrically between VCM + 0.5 V and VCM – 0.5 V, resulting in a 2-VPP differential input swing.
Can you please explain how +0.5V and -0.5V with respect to VCM will give 2-VPP?
Please explain with waveform.
Regards,
B Sandeep.