Part Number: ADS1263
Hi Team
Since the ADS1263 IDAC has a wide tolerance (max ±4%) we are using an external resistor to calibrate it. For example, we set IDAC1 to output 1mA, put this through a 1K calibration resistor (R8 below) and read back ~1V as expected.
The issue we are seeing is that when we set IDAC1 to 3mA, we only see ~2.5V across the 1K calibration resistor... instead of the expected ~3V.

Digging through the datasheet I see comments like below. Does this mean max IDAC current is actually limited by the internal 2.5V reference, and if we want to calibrate at 3mA then we need to reduce the calibration resistor to <833R (2.5V / 3mA)? Or have we made a silly mistake in our ADC configuration/conversion? 


Cheers, Anton