This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

TSW14J58EVM: TX IQ data wrap around problem using TRF1208-AFE7950EVM

Part Number: TSW14J58EVM

We are using the TSW14J58EVM and TRF1208-AFE7950EVM and have connected a RF loopback from TXA to RXA.

Latte v2.5 is used for setup and playback and capture of IQ data.

The problem we have is that there is a wrap around issue in the playback of IQ data. Playback of the IQ data buffer is not seamless, there is a discontinuity in the TX data.

When the TX IQ data wraps around from the end of the IQ data buffer to the start of the buffer there are 2 samples missing.
In the image below the data wrap around point is at x=101 so there seem to be some filter effects involved as well.
The TX IQ data is loaded using the command <setupParams.FPGA.sendCustomComplexData(0,filePath + fileName)>.

How can we solve this problem?