This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

DAC80508: Understanding and Calculating the total noise for a DAC output

Part Number: DAC80508


Hello,

I am a bit confused about calculating the total noise from the DAC Outputs. Specifically I don't understand this table

(Can be found on page 8 of the datasheet)

I think it is first telling the noise over the bandwidth of 0.1Hz to 10 Hz at 14uV. Then it specifies over larger bandwidths but how can the 10kHz noise bandwidth be lower than the 1kHz bandwidth? Are they meant to be taken together to get a total noise i.e. when the gain is 1 55 nV/sqrt(Hz) should be used from 1 kHz to 10kHz and then 50 from that point on. Also isn't 55 far lower than the graph shown on page 18 of the data sheet.

Any help would be greatly appreciated