Part Number: AFE5808A
I am interested in using the external reference mode of the AFE5808A. Do I understand correctly that this will shift the common mode of the internal pipeline ADCs, and that if I want to shift the common mode by 40% of the ADC range (so that an open input will yield an output of ~10% greater than the smallest possible numerical ADC output) I should set the voltage at pin M3 to 0.4V?
The data sheet also refers to an external reference current, but I don't see a description of how this would be used (what pin to connect to, for instance)... I'm probably just not looking carefully enough. I don't think I want to use an external current, but I'm curious about how I would do so and when I might want to.