Dear Technical Support Team,
I'd like to measure 2cases range of temperature with 3-Wire RTD for PT100.
①0℃~150℃ ⇒ 100Ω~157.33Ω
②0~400℃ ⇒ 100~247.09Ω(Expand from ①157.33Ω to 247.09Ω)
Q1
Is it necessary to change settings (gain, etc.) according to the range of resistance change?
I would like to know the settings to prevent accuracy deterioration due to an increase in the measurement range from ① to ②.
Q2
If the measurement resistance change range 100 to 157.33Ω is expanded to 100 to 247.09Ω, is it necessary to change the input circuit constants, etc.?
I would like to know the settings to prevent accuracy deterioration due to an increase in the measurement range from ① to ②.
My 3-Wire RTD HW configuration is copied from EVM.

■Following is my understanding.
ADS1x4S08 Evaluation Module(SBAU272A) page 21 shows following formula.
RRTD = (2 × R68 × ResultCODES / PGA ) / (2^24 – 1)
RREF=R68=1kΩ、PGA=4、Code=FullScale=7FFFFF(HEX)
Then max measurement range of RRTD is 250Ω.
It can cover the range of ① and ②, and it seems the best configuration to measure the range of ① and ②.
However if you have the best configuration for each ① and ②, please let me know.
| R68 | 1000 | Ω |
| ResultCODES | 8388607(DEC) | 7FFFFF(HEX) |
| PGA | 4 | |
| RRTD | 250 | Ω |
Best Regards,
ttd