This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

Analog Input IC(ADC) for PLC

Hello Team,

I hope this message finds you well. My name is Chhaya Mane and I represent Inditronics, an electronic product development and manufacturing company with a strong track record in delivering successful projects
Please find the below parts  for Project-IndiV7

Application :- Industrial IOT

Please find the required specification for below :

Analog Input IC(ADC) for PLC
Parameter Requirments
Resoluions 12 bits or 14 bits or 16Bits
No. of Channel 8 or 16 
Intrigrated AFE for Current  Input range 4 to 20mA, 0 to 20mA
Intrigrated AFE for Voltage Input range ±10V, ±5V, +5V,+10V
Sensing Accuracy ±0.3%
Interface Protocal  SPI(>=10MHz)
ESD Protections 8KV
Application PLC