Other Parts Discussed in Thread: LMK04828, ADC12DJ3200
I am using ADC12DJ3200EVM board. I would like to understand the procedure to generate one-shot SYSREF in subclass 1. Configuration value is given below
L = 4
M = 4
F = 8
Data Rate = 5Gbps
Also, I want to understand after power is turned on, when ADC converter samples the SYSREF incase of one-shot mode or in continuous or periodic mode? I need to add delay in generation of the SYSREF after power cycle? I refer below link but still not clear how to configure the different parameter infarct some parameters are not editable.
https://www.ti.com/lit/ta/ssztcl6/ssztcl6.pdf
Can you please, guide me on above query?