This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

ADS5409EVM: TSW1400EVM Firmware Permanently Update

Part Number: ADS5409EVM

Hello, is there a chance to set the default firmware for the TSW1400EVM Capture Card? Can I permanently load one of the RBF firmwares onto this kit using HSDC Pro or a different GUI? If I can't load it, which SPI pins are used for firmware update? Do you have any documentation regarding firmware updates? I'm developing a library to transfer data from TSW1400EVM to a Linux device, and I need this information.