Part Number: AFE5832LP
Other Parts Discussed in Thread: AFE5832,
When I used the test mode of AFE5832, I used the toggle mode. Why is the output of the AFE chip correct at the beginning of a short period of time, but after a while it becomes very messy?
In addition, when I used the AFE chip's all-0 or all-1 test mode, it was the same situation, only in the beginning of a period of time, the output of each channel of AFE was correct, and then the data changed not all 0 or all 1, but a jumble of numbers. What do you think is the reason? Does the AFE chip fail some time after writing to the register and setting to test mode? If this is the case, what should I do?