Part Number: DDC264
Hi teams. I have a concern about the analog input pin sorting order, such as IN1 to IN64. I'm going to design a linear detector with DDC264. With the other manufacturer ADC, I had a trouble according to cross talk between analog input pins. It was caused by the interaction within the chip. Then I dealed with mattching the pin name and the photo diode order. If DDC264 can also interact between analog input pins in the internal, should I match the pins such as IN1 to In64 and the photo diode order of linear detector to take better images?