Hi,
I'm currently trying to use an ADC3643EVM but when I check the DCLK output pin with an oscilloscope, this is what I see:

It's a very slow frequency signal, since the measurement is between -10ms and ~15ms.
Is there a problem with my card or is it just because I haven't configured it properly (I'm not configuring anything, just using the default configuration).
Here is my setup :

Thanks.