Part Number: ADS1298RECGFE-PDK
Other Parts Discussed in Thread: ADS1298R
Greetings,
I am using ADS1298R Eval kit. I am only using CHN-2 as Lead-1 and CHN-3 as Lead-2. I gave random data as input to check if the data is properly logged or not.
Method-1: I saved data as below in Excel,

Method-2: I saved data from 'Save' tab as well,

I've attached the log files. My observations are as below:
1) There is no option to Save Lead-3 and Augmented leads data in the Save tab.
2) For Lead-1 (CHN-2) and Lead-2 (CHN-3) data acquired from Method-2 have offset when compared with data acquired from Method-3.
My question now is,
1) How can I save Lead-3 and Augmented leads data?
2) Is it still possible both methods (Exporting from Plot and Saving in the tab) are showing same data but with some offset? How much offset is added?
Please suggest a method or a document we could refer to understand the above points.
Thank you,
V. Vedashree