Hi, i''ve purchased a Ti's evaluation board for the AD converter ADS 1232 REF and i've been having some problems.
When I try to connect the board with the PC through the TI's software it's supposed to show "scanning" in the status during the port test and then it must show the number of the COM port that are connected. When I connect the board I can see the "scanning" in the status but neither show a single COM nor gets out of the "scanning" state.
I tried to connect the board though the hyperterminal and the board sent the version of the program so I'm sure that the communication with the board is possible.
I'm running on a windows XP machine with the drivers correctly instaled (i've checked when I connect the board that the USB module is recognized and a COM port is assigned to it)
Is there any ideas of what's going on? Any way of solve this problem?
Thank you
Alejandro