Part Number: ADS8166
Hello,
My customer is interested in using ADS8166 with DVDD = 1.8V, however, the device states that it's specified DVDD is from 2.35V to 5.5V (3V typical) even though it's operating DVDD is from 1.65V to 5.5V (3V typical).
Do you have any concerns regarding using DVDD = 1.8V? Is there anything they'd need to watch out for?
I did see other E2E post where TI was recommending eliminating voltage level translators and using DVDD = 1.8V for the ADS816x, so this appears to be an acceptable use case.
The datasheet is also missing the digital input and output levels (Vih/l and Voh/l). For DVDD = 1.8V, should they use 0.8*DVDD for Vih/Voh min and 0.2*DVDD for Vil/Vol max? This seems to align with the conditions in the fclk spec (serial clock frequency) of 20MHz max for SPI interface. However, there's no indication for what to expect for Voh/Vol.
Thanks in advance for your support.
Best Regards,
Brian Gosselin