Part Number: DAC1282
Hi, I'm just trying to get some clarification on setting up a DAC1282 with a custom pcb board that uses a stm32 F7 series chip.
First question:
From reading the data sheet it says the SPI interface is a half duplex system yet in all of the diagrams and figures in the datasheet is clearly shows that it has both a DIN and a DOUT line in the communication figures and in the pinout. I thought half duplex implied there was only one shared data line? Or would I still implement it as a full duplex and just not use the TransmitReceive command? im fairly confused about how all of this would work because everything else half duplex related only shows one data line that I've seen.
Second question:
What SPI mode would this need to be in to operate successfully? From the data sheet it says high or low for polarity and "Data are input on the serial clock (SCLK) rising edge and output on the SCLK falling edge" for the clock phase so would that be SPI mode 0 and 2 are valid options or do I have that backwards?
The biggest issue I'm currently trying to solve is that my data on the logic analyzer always either seems to shift left, shift right, lose the last bit, lose the first bit, or give me zero when it shouldn't depending on which SPI mode I set it as in the MCU settings. This is all on the MOSI line trying to send opcodes to read some of the config registers. I'm sure it's probably a combination of improper SPI settings along with something else I'm overlooking but instead of trying to brute force my way though I thought I would ask the experts. Thank you in advance for taking the time to answer my questions.