This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

ADS127L21: About input current

Part Number: ADS127L21

I am having trouble with the large input current of the IC.

AVDD1 = 5V
AVDD2 = 5V
AVSS = 0V
REFP = 2.5V
REFN = 0V
IOVDD = 3.3V
OSR 1024

AINP=4.5V Current 350uA
AINN=0.5V Current 350uA

Since the input current is large as mentioned above,
The voltage drop is large and measurement accuracy is poor.
The datasheet says 4uA.
Does anyone know?