Part Number: ADS1231
Other Parts Discussed in Thread: ADS1230, ADS1232, ADS1220
Hi,
How to change the gain of the internal amplifier present in the ADS1231.

This thread has been locked.
If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.
Hi Murugavel S,
Please refer to the ADS1231 datasheet. This device has a fixed gain of 128 only. Another single-channel option would be the ADS1230 which has gain options of 64 and 128 but with slightly lower resolution. The ADS1232 is a two channel 24-bit ADC with gain options of 1, 2, 64 and 128. All of these devices are pin controlled for gain settings.
If you need additional gain options you could also consider the ADS1220.
Best regards,
Bob B