This thread has been locked.
If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.
I have a system that uses the ads1293 and it works well. I want to add respiration so I want to
run a 1292R chip in sync with the 1293..
I this possible ? is it a good idea ?
The data sheets tell how to sync multiple ads1293 OR multiple 1292R but not
one of each.
thanks
phil
Hi Phil,
It is not recommended to combine ADS1292R and ADS1293 since clocking is different and the devices do not support daisy chaining them together.
How many ECG channels do you require for your application?
You can consider ADS1294R which will have 3 ECG channel and 1 respiration channel.