Hi All,
I connect TSW3100 to our CMOS board and it produces kind of modulated signal.
All LED of TSW3100 lit up properly for CMOS Patterns. ( D13,14,15,19,20,21)
1) TSW 3100 GUI does not run if "interleaved" is not checked.
1) IF signal appears to have on wrong format. I tied both : two's compliment and offset bin.
2) Can anyone suggest what could be the causes. Attached are IF signal and TSW GUI settings.
thks,thu


Zoom in