I would like to use this part with Versal FPGAs from AMD/Xilinx which have 1.5V max I/O bank voltages, but noticed that this part's VDDIO has a recommended range of 1.71 to 1.89V. Is it possible to operate VDDIO at 1.5V logic levels? If so, are there any special power sequencing considerations when doing this?