Hi team,
Please tell me about slave addresses.
Power is applied to AVDD, and the state of the ADDR pin is captured at the timing of POR release, at which point it is determined.
After the slave address is fixed, there is no change in the slave address even if the state of the ADDR pin changes.
Is this correct?
If so, how long is the POR time?
Is it about 50us of "Power-up time" after the AVDD voltage of the operating voltage becomes about 2.7V?
Sincerely,
Ryu.