This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

AFE58JD48: test

Part Number: AFE58JD48

hello,
     I am using FPGA to configure AFE58JD48. I want to verify the JESD204B link. However, after configuring some registers, I found that the JESD204B IP CORE in the FPGA did not show any received data. Please help to confirm if my register configuration is correct.
    FPGA side, I found rx_islockedtodata signal is always 0 , this should indicate that  JESD204B IP core cannot recover clock from serial data by CDR.
 Here is my current register configuration:
Begin
SPI_DIG_EN = 1     00_0001 #  global reset, self clear
SPI_DIG_EN = 1     C5_4000 #  according to "12.2 Device initialization"
SPI_DIG_EN = 1     D0_0001 #
SPI_DIG_EN = 1     DE_00C3 #
SPI_DIG_EN = 1     DF_0040 #
SPI_DIG_EN = 1     1E_0003 #
SPI_DIG_EN = 1     12_0005 #
SPI_DIG_EN = 1     2A_0800 #
SPI_DIG_EN = 1     12_0000 #
SPI_DIG_EN = 1     11_FFFF #
SPI_DIG_EN = 1     25_0002 #
SPI_DIG_EN = 1     11_0000 #
SPI_DIG_EN = 1     12_000A # according to "10.3.8.1.2 JESD 80X Mode (or 4-Lane Mode)" NOTE
SPI_DIG_EN = 1     29_0001 #
SPI_DIG_EN = 1     31_03C0 #
SPI_DIG_EN = 1     34_091F #
SPI_DIG_EN = 1     35_01C0 #
SPI_DIG_EN = 1     36_0007 #
SPI_DIG_EN = 1     30_8002 #
SPI_DIG_EN = 1     30_8006 #
 
SPI_DIG_EN = 1     31_03D0 # test
SPI_DIG_EN = 1     32_0040 # 
SPI_DIG_EN = 1     12_0000 #
End
thanks!