This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

DAC38RF84: Vout1 open circuit condition

Part Number: DAC38RF84


With DAC38RF84 configured for an output level of -7dBm (∼0.1 V)

There was an unintentional open circuit termination at the output of the device.

This causes the output power to be fully reflected back to the device at 2x the magnitude (∼0.2V).

The maximum ratings for the DAC38RF84 per the data sheet at Vout1+/- or Vout2+/- are: -0.5 V min to VDDAOUT18+0.5V max.

Where, VDDAOUT18 = 1.8V (DAC Supply voltage). 

The reflected voltage is within the allowable voltage tolerance for the Vout interface however, is it possible the DAC output is damaged possibly exhibiting as a drifting output level?