Part Number: AFE58JD28
Hi Tier
My customer use AFE58JD28 to do Power-down function and wake up then go to the power-up recovery phase.
They found the AFE58JD28 do not wake up during 15ms.
So we would like to understand the detail:
1. What is the maximum number of seconds for the recovery time of Power up? 15 ms seems inaccurate.
I see that the manual says that the maximum wake-up time depends on the capacitance on the INM INP, and I'll ask the customer to check that, right?
2. If chip power up by customer , do we need to reconfigure any registers?
3. Do we need to send a sync trigger after power up to successfully wake up the device?
Thank you very much.