Hi,
The customer is testing the ADS7957QDBTRQ1 circuit after designing it.
The Max value should be output when it is about 5V input based on the ADC 1024 value with the 10bit resolution specification.
Currently, the Max value is coming out at about 1.5V input level.
I would like to ask if there are any additional parts that need to be set up.