This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

ADC128S102-SEP: The ADC is saturating at 4.5V

Part Number: ADC128S102-SEP


Hello, 

I am using ADC128S102-SEP in one of our design and we realized that the ADC reading is saturating around 4.5V. Wanted to check if this is true or there is some failure in our case also we are using a unity gain opamp LMP2012WG-QMLV before the Analog input. The Va is supplied with 5V and the Vd is at 3.3V and the OPAMP is powered by same 5V rail. 

For the input of the OPAMP we have a potential divider and lower divider is a "pot" for doing this sweep. It would be great if you can give me some input on the issue.