This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

TLA2528: DVDD powered with no AVDD

Part Number: TLA2528


Customer has a condition where the DVDD pin will be powered with 1.8V, but AVDD is not yet powered. Is this a concern for the TLA2528?

 Note that the Ain inputs are not present during this condition so the inputs are not > AVDD. AVDD is normally 3.3V when powered.