Part Number: ADS1278
Dear TI,
I am looking for space qualified multi-channel ADC. I need to sample very low bandwidth signals (carrier waves) with carrier frequencies of ~10 MHz.
I am wondering whether ADS1278 (which has maximum sampling rate of 144 kHz) could be used to sample these ~10MHz signals in under-sampling mode.
What would be your opinion about this idea?
Have you characterized the input analog bandwidth of this chip up to 10 MHz (or even more)?
Is it in general a bad idea to use sigma-delta ADC for doing undersampling?
(I am considering this particular ADC, since you also provide it in a space-qualified version, and we are targeting a space application on Medium Earth Orbit. Unfortunately, I could not find many multi-channel (ideally 8 channels, 4 would be acceptable) space-qualified ADCs with sampling frequencies allowing to directly sample these ~10MHz signals.)
Thank you very much!
Ondrej