Other Parts Discussed in Thread: ADS127L11
Hi,
we are trying to make it work the ADC ADS1258 to assess its suitability for future projects. To facilitate this, we have developed a custom board to accommodate the geometric constraints of our testing environment, and we have connected it according to the configuration depicted in the attached image.

Our objective is to directly acquire data from the ADCINN and ADCINP pins, bypassing the internal multiplexer.
We have proceeded to establish communication with the ADC using an Arduino UNO, following both the instructions outlined in the datasheet and the example code provided. With the help of scope, we have confirmed that MISO, MOSI, and SCLK are all functioning as expected, with DRDY toggling as foreseen.
The code employed for this purpose is as follows:
#include <SPI.h>
#define CS_PIN 10 // Chip select pin for ADS1258
const int DRDY=2;
byte stat,data1,data2,data3;
float dataF;
void setup() {
Serial.begin(9600); // Initialize serial communication
pinMode(CS_PIN, OUTPUT); // Set CS pin as output
// Initialize SPI communication
SPI.begin();
SPI.setClockDivider(SPI_CLOCK_DIV16); // Set SPI clock frequency (16 MHz / 16 = 1 MHz)
// Initialize ADS1258
digitalWrite(CS_PIN, HIGH); // Deselect ADS1258
delay(100); // Delay for stable operation
digitalWrite(CS_PIN, LOW); // Select ADS1258
// Send configuration commands to ADS1258
SPI.transfer(0xC0); // Send command: reset
delay(100); // Delay for reset to complete
digitalWrite(CS_PIN, HIGH); // Deselect ADS1258
digitalWrite(CS_PIN, LOW); // Select ADS1258
// Configure ADS1258 settings for single-ended operation (example settings, adjust as needed)
SPI.transfer(0x60); // Send command: write register
SPI.transfer(0x3A); // Send value to write: CTRL0 register value (example: PGA = 1, SPS = 30)
digitalWrite(CS_PIN, HIGH); // Deselect ADS1258
digitalWrite(CS_PIN, LOW); // Select ADS1258
// Configure MUX register to select ADCINN and ADCINP as input channels directly
SPI.transfer(0x62); // Send command: write register
SPI.transfer(0x17); // Send value to write: CTRL0 register value (example: PGA = 1, SPS = 30)
digitalWrite(CS_PIN, HIGH); // Deselect ADS1258
digitalWrite(CS_PIN, LOW); // Select ADS1258
// Configure MUX register to select ADCINN and ADCINP as input channels directly
uint8_t read= SPI.transfer(0x50);
read= SPI.transfer(0x00);
Serial.print("register control0:");
Serial.println(read,HEX);
Serial.println(read,HEX);
read= SPI.transfer(0x00);
Serial.print("register control1:");
Serial.println(read,HEX);
Serial.println(read,HEX);
read= SPI.transfer(0x00);
Serial.print("register control2:");
Serial.println(read,HEX);
// Deselect ADS1258
digitalWrite(CS_PIN, HIGH);
digitalWrite(CS_PIN, LOW);
uint8_t stat=SPI.transfer(0x00);
}
void loop() {
// Select ADS1258
digitalWrite(CS_PIN, LOW);
// Send command to read data
SPI.transfer(0x01); // Send command: read register
SPI.transfer(0x12); // Send register address: DATA register
delay(1); // Delay for conversion
SPI.transfer(0x00) << 16; // Read MSB
// Read data from ADS1258
if (digitalRead(DRDY)==LOW)
{
delayMicroseconds(30);
int32_t rawValue = 0;
//uint8_t stat=SPI.transfer(0x00);
rawValue |= SPI.transfer(0x00) << 16; // Read MSB
rawValue |= SPI.transfer(0x00) << 8; // Read middle byte
rawValue |= SPI.transfer(0x00); // Read LSB
// Deselect ADS1258
digitalWrite(CS_PIN, HIGH);
// Convert raw value to voltage (example: assuming Vref = 5V, 24-bit resolution)
float voltage = (5.0 / 7864320.0) * rawValue; // Vref / (2^24) * rawValue786432
// Print voltage value to serial monitor
// Serial.print("Voltage: ");
Serial.println(rawValue,HEX);
// Serial.println(" V");
//Serial.println(stat,HEX);
// Delay before next reading
delay(100);
}
}
However, the communication seems completely wrong. reading the control registers we do not obtain the default values and if we try to write new values in the control registers for bypassing the internal mux and fixing one channel of the mux to not scan over the internal signals, at the next reading of the control register the value is different from the one sent over SPI (sent burst verified with a scope). Also, the converted data seems wrong and does not respond to changes in the applied input voltage.
Do you notice any issues with our approach?
We have also experimented with the libraries in the example code but encountered the same outcome. Even a simple reading of control0 at startup fails to display 0x0A as expected.
Thank you very much for any insights you may be able to provide.
Best regards,
Vincenzo