This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

LM98640CVAL: Support files for the Aardvark SPI host adapter provided with the LM98640CVAL Evaluation Board

Part Number: LM98640CVAL

Hi,

We are requesting support files to utilize with the SPI host adapter that was supplied with the LM98640CVAL Evaluation Board.  Supplied with the Eval board was a Total Phase Aardvark I2C/SPI Host Adapter.  The LM98640CVAL Evaluation Board did not come with any software or files.  We can get the operating software for the Host adapter from Total phase but I am asking for specific scripts or other files or specific instructions that specify the setup and/or control the LM98640CVAL Evaluation Board specifically using the Aardvark I2C/SPI Host Adapter.  Please provide support so that we can use the supplied Aardvark I2C/SPI Host Adapter.

Thank you!

Scott Thomas

sthomas@iristechnology.com

949-338-8463