This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

AFE882H1EVM: IOVDD current consumption related issue

Part Number: AFE882H1EVM
Other Parts Discussed in Thread: AFE882H1

Hi team,

One of my customer is working on one of the project for which AFE882H1 & evaluating with EVM. They observed that IOVDD (1.8V external) supply consumption is 195uA instead of 10uA as mentioned in datasheet.

Following is the test conditions.

    1. All other ICs from board removed except AFE882H1.
    2. PVDD is 3.5V provided from other hardware and consumption is 210uA.
    3. IOVDD is 1.8V provided from other hardware and consumption is 195uA.
    4. Ground wire shorted between microcontroller board and AFE eval board, so only one ground reference for both boards.
    5. All respective jumpers removed from board except J6 for internal filter.
    6. HART is working well.

Can you help here? What is the issue for higher current on IoVDD line?

Regards,

Mitesh